ACTION#.SOURCEID
Description
Some action sources require a specific source ID number. For example, if your action source is a Digital Input, then a source ID of 1 would correspond to Digital Input 1.
The range of the source ID will depend on the value of the corresponding source. If the source is modified, the range and units of the source ID may change, and the source ID value will default to the first valid value.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Depends on ACTION#.SOURCE |
Range |
Depends on ACTION#.SOURCE |
Default Value |
0 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
ACTION1.SOURCEID |
3905h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION2.SOURCEID |
3905h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION3.SOURCEID |
3905h |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION4.SOURCEID |
3905h |
04h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION5.SOURCEID |
3905h |
05h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION6.SOURCEID |
3905h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION7.SOURCEID |
3905h |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION8.SOURCEID |
3905h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION9.SOURCEID |
3905h |
09h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION10.SOURCEID |
3905h |
0ah |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION11.SOURCEID |
3905h |
0bh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION12.SOURCEID |
3905h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION13.SOURCEID |
3905h |
0dh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION14.SOURCEID |
3905h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION15.SOURCEID |
3905h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION16.SOURCEID |
3905h |
10h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION17.SOURCEID |
3905h |
11h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION18.SOURCEID |
3905h |
12h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION19.SOURCEID |
3905h |
13h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION20.SOURCEID |
3905h |
14h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION21.SOURCEID |
3905h |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION22.SOURCEID |
3905h |
16h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION23.SOURCEID |
3905h |
17h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION24.SOURCEID |
3905h |
18h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION25.SOURCEID |
3905h |
19h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION26.SOURCEID |
3905h |
1ah |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION27.SOURCEID |
3905h |
1bh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION28.SOURCEID |
3905h |
1ch |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION29.SOURCEID |
3905h |
1dh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION30.SOURCEID |
3905h |
1eh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION31.SOURCEID |
3905h |
1fh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION32.SOURCEID |
3905h |
20h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
ACTION1.SOURCEID |
40600 |
9E98 |
Unsigned8 |
Read/Write |
- |
ACTION2.SOURCEID |
40601 |
9E99 |
Unsigned8 |
Read/Write |
- |
ACTION3.SOURCEID |
40602 |
9E9A |
Unsigned8 |
Read/Write |
- |
ACTION4.SOURCEID |
40603 |
9E9B |
Unsigned8 |
Read/Write |
- |
ACTION5.SOURCEID |
40604 |
9E9C |
Unsigned8 |
Read/Write |
- |
ACTION6.SOURCEID |
40605 |
9E9D |
Unsigned8 |
Read/Write |
- |
ACTION7.SOURCEID |
40606 |
9E9E |
Unsigned8 |
Read/Write |
- |
ACTION8.SOURCEID |
40607 |
9E9F |
Unsigned8 |
Read/Write |
- |
ACTION9.SOURCEID |
40608 |
9EA0 |
Unsigned8 |
Read/Write |
- |
ACTION10.SOURCEID |
40609 |
9EA1 |
Unsigned8 |
Read/Write |
- |
ACTION11.SOURCEID |
40610 |
9EA2 |
Unsigned8 |
Read/Write |
- |
ACTION12.SOURCEID |
40611 |
9EA3 |
Unsigned8 |
Read/Write |
- |
ACTION13.SOURCEID |
40612 |
9EA4 |
Unsigned8 |
Read/Write |
- |
ACTION14.SOURCEID |
40613 |
9EA5 |
Unsigned8 |
Read/Write |
- |
ACTION15.SOURCEID |
40614 |
9EA6 |
Unsigned8 |
Read/Write |
- |
ACTION16.SOURCEID |
40615 |
9EA7 |
Unsigned8 |
Read/Write |
- |
ACTION17.SOURCEID |
40616 |
9EA8 |
Unsigned8 |
Read/Write |
- |
ACTION18.SOURCEID |
40617 |
9EA9 |
Unsigned8 |
Read/Write |
- |
ACTION19.SOURCEID |
40618 |
9EAA |
Unsigned8 |
Read/Write |
- |
ACTION20.SOURCEID |
40619 |
9EAB |
Unsigned8 |
Read/Write |
- |
ACTION21.SOURCEID |
40620 |
9EAC |
Unsigned8 |
Read/Write |
- |
ACTION22.SOURCEID |
40621 |
9EAD |
Unsigned8 |
Read/Write |
- |
ACTION23.SOURCEID |
40622 |
9EAE |
Unsigned8 |
Read/Write |
- |
ACTION24.SOURCEID |
40623 |
9EAF |
Unsigned8 |
Read/Write |
- |
ACTION25.SOURCEID |
40624 |
9EB0 |
Unsigned8 |
Read/Write |
- |
ACTION26.SOURCEID |
40625 |
9EB1 |
Unsigned8 |
Read/Write |
- |
ACTION27.SOURCEID |
40626 |
9EB2 |
Unsigned8 |
Read/Write |
- |
ACTION28.SOURCEID |
40627 |
9EB3 |
Unsigned8 |
Read/Write |
- |
ACTION29.SOURCEID |
40628 |
9EB4 |
Unsigned8 |
Read/Write |
- |
ACTION30.SOURCEID |
40629 |
9EB5 |
Unsigned8 |
Read/Write |
- |
ACTION31.SOURCEID |
40630 |
9EB6 |
Unsigned8 |
Read/Write |
- |
ACTION32.SOURCEID |
40631 |
9EB7 |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
ACTION1.SOURCEID |
40600 |
Unsigned8 |
Read/Write |
- |
ACTION2.SOURCEID |
40601 |
Unsigned8 |
Read/Write |
- |
ACTION3.SOURCEID |
40602 |
Unsigned8 |
Read/Write |
- |
ACTION4.SOURCEID |
40603 |
Unsigned8 |
Read/Write |
- |
ACTION5.SOURCEID |
40604 |
Unsigned8 |
Read/Write |
- |
ACTION6.SOURCEID |
40605 |
Unsigned8 |
Read/Write |
- |
ACTION7.SOURCEID |
40606 |
Unsigned8 |
Read/Write |
- |
ACTION8.SOURCEID |
40607 |
Unsigned8 |
Read/Write |
- |
ACTION9.SOURCEID |
40608 |
Unsigned8 |
Read/Write |
- |
ACTION10.SOURCEID |
40609 |
Unsigned8 |
Read/Write |
- |
ACTION11.SOURCEID |
40610 |
Unsigned8 |
Read/Write |
- |
ACTION12.SOURCEID |
40611 |
Unsigned8 |
Read/Write |
- |
ACTION13.SOURCEID |
40612 |
Unsigned8 |
Read/Write |
- |
ACTION14.SOURCEID |
40613 |
Unsigned8 |
Read/Write |
- |
ACTION15.SOURCEID |
40614 |
Unsigned8 |
Read/Write |
- |
ACTION16.SOURCEID |
40615 |
Unsigned8 |
Read/Write |
- |
ACTION17.SOURCEID |
40616 |
Unsigned8 |
Read/Write |
- |
ACTION18.SOURCEID |
40617 |
Unsigned8 |
Read/Write |
- |
ACTION19.SOURCEID |
40618 |
Unsigned8 |
Read/Write |
- |
ACTION20.SOURCEID |
40619 |
Unsigned8 |
Read/Write |
- |
ACTION21.SOURCEID |
40620 |
Unsigned8 |
Read/Write |
- |
ACTION22.SOURCEID |
40621 |
Unsigned8 |
Read/Write |
- |
ACTION23.SOURCEID |
40622 |
Unsigned8 |
Read/Write |
- |
ACTION24.SOURCEID |
40623 |
Unsigned8 |
Read/Write |
- |
ACTION25.SOURCEID |
40624 |
Unsigned8 |
Read/Write |
- |
ACTION26.SOURCEID |
40625 |
Unsigned8 |
Read/Write |
- |
ACTION27.SOURCEID |
40626 |
Unsigned8 |
Read/Write |
- |
ACTION28.SOURCEID |
40627 |
Unsigned8 |
Read/Write |
- |
ACTION29.SOURCEID |
40628 |
Unsigned8 |
Read/Write |
- |
ACTION30.SOURCEID |
40629 |
Unsigned8 |
Read/Write |
- |
ACTION31.SOURCEID |
40630 |
Unsigned8 |
Read/Write |
- |
ACTION32.SOURCEID |
40631 |
Unsigned8 |
Read/Write |
- |